The CasaLink Block Terminal (CBT) is a pre-connectorised, compact box, easily mounted on the wall or on a pole. The CBT system does not use a proprietary drop or feeder cable, Prysmian’s patented fibre locking system allows loose tube cables can be utilised with existing overhead infrastructure.
CBT can be used as part of a point to point or PON system, so balanced or unbalanced splitters can be pre-installed within the block, increasing the capacity of the fibres accommodated within its compact size.