HV and Submarine Power Transmission

OVERVIEW

Linking worldwide progress to global power

To countries, to cities, to homes. On land and under the seas. Prysmian is bringing power and communications to the world. As the demand for both continues to soar and industries move steadily towards more renewable and sustainable energy sources, Transmission System Operators (TSOs) are increasingly engaged in developing, extending and upgrading their power grids. This involves the transmission of power via interconnectors that stretch across land and under seas, between countries and continents.

Our commitment to the energy transition

The transition from fossil fuels to renewable energy requires an efficient, smart, and robust energy grid to meet the special challenges of managing these discontinuous power sources. Interconnectors are an increasingly important part of power grids, allowing for connections between countries and even continents to ease the flow of affordable and clean energy across long distances. They are a key part of the energy transition: supporting the implementation of a larger, more integrated, efficient and sustainable power transmission system. Prysmian’s submarine interconnectors are made of new, lighter materials and can go deeper under the sea than ever before. Our high-voltage underground interconnectors can bring power more efficiently over long distances from where the energy is produced (like offshore wind farms) to where energy is consumed. To accelerate the race to net-zero CO2 emissions, Prysmian plans to invest over 450 million euro by 2022 to further improve the sustainability of its organization and supply chain, and to accelerate the development of advanced cable technologies as well as assets and services.

An Innovation leader

Prysmian is an innovation leader in both high-voltage submarine and underground cable system. Our Research and Development labs have created a submarine cable with new synthetic armour which can be up to 50% lighter than others, enabling Prysmian to perform ultra-deep installations or up to 3,000 meters in marine ecosystems previously considered impossible. For underground power transmission, we have designed new ±525 kV HVDC cable systems, qualified with P-Laser and XLPE insulation, with a higher voltage capacity and with large conductor cross-sections to provide optimal technical solutions for more efficient, reliable and eco-friendly power transmission over long distances.

VIDEO

Leonardo da Vinci – a genius in motion

Prysmian has built a fourth vessel, Leonardo da Vinci, that reinforces the fleet. This new strategic asset will consolidate the Group’s leadership in the submarine cable operations, strengthening our primary role in the interconnection and offshore wind farm markets.

PROJECTS

A deep dive into the power transmission cable and systems world.

Undisputed world leader in the provision of HV underground & Submarine Transmission cables

We’re the strategic partners for our TSO customers, supporting the development and production of transmission grids, and helping to facilitate the bulk movement of electrical energy from the site of generation to electrical substations. Making innovation a cornerstone of our work, and R&D a constant investment, we offer both HVAC and HVDC cable systems for power transmission for both land and submarine connections.

But we deliver so much more… following the integration of General Cable into Prysmian, we can now call on the strength of NSW and its longstanding expertise in fibre-optic submarine cables, accessories and solutions.

VIDEO

Underground cable solutions

A deep dive into Prysmian High Voltage underground cables system and solution. Prysmian is the undisputed leader in high voltage land cable systems and solutions that are fundamental parts of power grids across the world.

So we’re now better placed than ever to work in close partnership world-leading network operators as they look to establish the next generation of communications infrastructure. Fundamentally, our customers require products and solutions that offer the lowest possible environmental impact and the highest added value – along with uncompromising safety and reliability. And that’s exactly what we provide.

NSW

Submarine Telecoms Solutions

The transmission of data and communications has long stretched beyond the confines of the land. In response to an ever-growing requirement for telecommunications to be transmitted across oceans, Prysmian has expanded its reach to once again become a world leader.
With the acquisition of General Cable, Prysmian added the capability and services of Norddeutsche Seekabelwerke GmbH (NSW) to its portfolio. 

OUR MARKETS

Network Components

Applying years of experience, Prysmian offers a complete range of accessories for all types of energy cable. This is backed by specialist engineering services to help you fulfill any power system requirement or specification.

OUR MARKETS

Power From Shore

The offshore production of oil and gas plays a vital role in the energy infrastructure of many countries.

OUR MARKETS

Asset Monitoring Systems

In HV & Submarine power transmission grids cable systems represent a high-value asset to be preserved and each non-transmitted MW is a financial loss factor.

Our Strenghts


Product Technology Innovation

Product Technology Innovation

Product Technology Innovation
Installation Capabilities

Installation Capabilities

Installation Capabilities
Production Facilities

Production Facilities

Production Facilities
Project Excellence

Project Excellence

Project Excellence
Q&HSE management & Sustainability

Q&HSE management & Sustainability

Q&HSE management & Sustainability
Smart Monitoring & Maintenance

Smart Monitoring & Maintenance

Smart Monitoring & Maintenance